The following table describes the attributes used by the Pass Through (Boolean, Enum) modules.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Input |
The input to the pass through module. |
1st Enum or False |
|
Present Value |
G, V |
The output of the pass through module |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)