Module Use in Applications (Occupied Zone Sequencing [FC/AHU]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Occupied Zone Sequencing (FC) Uses in Application System Selection Trees

Module Instance Name

Applications

FC-ZN-T Sequencing v51

Fan Coil Applications

Zone Sequencing v51

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

AHU Rooftop Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.