Module Use in Applications (Occupied Sequencing [AHU MASD w HR]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Occupied Sequencing (AHU MASD w HR) Uses in Application System Selection Trees

Module Instance Name

Applications

Mixed Air Single Duct HR Sequencing v51

AHU Mixed Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.