Module Use in Applications (Occupied Sequencing [AHU MASD]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Occupied Sequencing (AHU MASD) Uses in Application System Selection Trees

Module Instance Name

Applications

Mixed Air Single Duct Sequencing v51

AHU Rooftop Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.