The application System Selection trees use the individual modules in this group using the names in the following table.
Module Instance Name |
Applications |
---|---|
Start Stop Sequencing |
|
Start Stop Sequencing DA-T |
AHU Mixed Air Single Duct Applications(DA-T Control) |
Start Stop Sequencing Zone |
AHU Mixed Air Single Duct Applications (Zone Control) |
To see a module's connections and how modules interact with it, view the Connections table.