Module Use in Applications (Loss of Airflow Sequencing) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Loss of Airflow Sequencing Uses in Application System Selection Trees

Module Instance Name

Applications

Loss of Airflow Sequencing

All Air Handling Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.