Module Use in Applications (Humidification Sequencing) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Humidification Sequencing Uses in Application System Selection Trees

Module Instance Name

Applications

Humidification Sequencing

All Air Handling Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.