The following table describes the attributes used by the Humidification Sequencing module.
Name |
Description |
Default Value |
---|---|---|
Discharge Humidity |
Contains the discharge air humidity. |
50.0%RH |
Discharge Humidity Setpoint |
Contains the discharge air high humidity setpoint. |
70.0%RH |
Humidity Control Status |
Value fed back from the humidification controller necessary for the sequencer to determine what actions to take. This input is the PID status from humidification output controller. |
Normal Set Name: Control Status |
Humidity Process Variable |
Contains the zone or the return air humidity. |
50.0%RH |
Humidity Setpoint |
Defines the zone or return air humidification setpoint. |
40.0%RH |
HUM-STATE (State) |
Current state generated by the AHU humidification sequence. |
No Humid Set Name: AHU Hum States |