Module Use in Applications (Dual Fan No Airflow Sequencing) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Dual Fan No Airflow Sequencing Uses in Application System Selection Trees

Module Instance Name

Application

Dual Fan Loss of Airflow Sequencing

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.