Module Use in Applications (Dehumidification Sequencing) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Dehumidification Sequencing Uses in Application System Selection Trees

Module Instance Name

Applications

Dehumidification Sequencing v3
Note: This module is also referred to as Dehumidification Sequencer v3.

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

AHU Rooftop Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.