Coil Circulation Pump Sequencing - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Coil Circulation Pump Sequencing provides Less Than or Equal logic. This logic block is laid down by the Coils > Coil Pump > Low Temperature Circulation selection in the Air Handling Unit Applications. If the Outdoor Air Temperature is less than the Low OA-T Setpoint, the pump is called to run. See the Less Than or Equal description in the Compare topic of the Logic section.

To see a module's connections and how modules interact with it, view the Connections table.