Attributes (Binary Override Check) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by the Analog Override Check module.

Table 1. Binary Override Check Attributes

Name

Type 1

Description

Default Value

Command n

 

Indicates the current command of the monitored BO.

Off (0)

Set Name: Off/On

Command n Priority

 

Indicates the current priority of the monitored BO.

0

Display Precision: 1s

Device Capacity

 

Indicates the percent capacity that each Command n represents. This value is used to calculate the Output Position.

12.5

Device Enable

 

Provides an enable signal used by an MSC or Sequencer module.When the matching Command n Priority is overridden, the output is False.When the matching Command n Priority is not overridden, the output is True.

False

Number of Input Attributes

 

Indicates the number of inputs evaluated by this module. The module calculates this value.

1

Output Overridden

G

Indicates whether the output is overridden.This output value is set to True when Setup equals AND, and all of the Command n Priority inputs show that the output objects being monitored are in an Overridden State (that is, the value is greater than zero and less than 16).This output value is set to True when Setup equals OR, and any of the Command n Priority inputs show that the output objects being monitored are in an Overridden State.

False

Output Position

 

Indicates the estimated PID command that produces the current state of the Command n inputs. This value is calculated as: (Total Inputs in State 1) x Device Capacity.

0.0

Setup

 

Indicates whether the value of Output Overridden is set to True when all of the Output n Priority inputs are not 0 or 16 (AND), or this value is set to True when any of the Output n Priority inputs are not 0 or 16 (OR).

OR

Set Name: AND/OR

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)