Reliability (Heat Recovery Suitability Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Heat Recovery Suitability output is set to None if the OA Temperature, Exhaust Air Temperature, or the Low Limit Process Variable inputs are not reliable.