Attributes (Tower Start Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Tower Start Determination modules:

Table 1. Tower Start Determination Attributes

Name

Type 1

Description

Default Value

isAvailable

 

Indicates whether the system is enabled.

False

Pump Count

 

Indicates the number of active pumps.

0

Pump Delay

 

Indicates the amount of time to wait after turning off pumps before closing isolation valves.

20 Seconds

State

G

Provides an output indicating whether the cooling tower subsystem is enabled.

False

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)