Module Use in Applications (Tower Sequencing-Vernier) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Tower Sequencing-Vernier Uses in Application System Selection Trees

Module Instance Name

Applications

On/Off Fan w/ Vernier Output Clg Twr Sequencing v50

Central Cooling Applications

To see a module's connections and how modules interact with it, view the Connections table.