System Enable - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The System Enable module enables or locks out a heating or cooling device. This module accepts as inputs outdoor air temperature, outdoor air enable setpoint, outdoor air enable differential, heating/cooling selection, and a network isAvailable. The module has a state output that indicates if the module is enabled.

You can view and modify the modules in this group’s logic.