Secondary Bypass Valve Sequencing - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This module is responsible for controlling the state of the secondary bypass valve PID, based on system enable and the output of the secondary pumping PID. This module is implemented as a standard Control Activity.

Figure 1. Secondary Bypass Valve Sequencing Module