Attributes (PID Sequencer) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the PID Sequencer modules:

Table 1. PID Sequencer Attributes

Name

Type 1

Description

Default Value

BYP Saturation

(Input 1)

 

Provides an input that comes from the Cooling Tower Valve Control Status output.

Disabled

Set Name: Control Status

CT Saturation

(Input 2)

 

Provides an input that comes from the Cooling Tower Fans Control Status output.

Disabled

Set Name: Control Status

Delay

 

Indicates the minimum time after a Stage Up that another operation (Stage Up or Stage Down) can be performed.

15

Display Units: Seconds

State

 

Indicates the current state generated.

Off

Set Name: Plant Sequencing Mode

System Enable

 

Enables the staging process to run using an Off/On command.

Disabled

Set Name: Disable Enable

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)