Module Use in Applications (Load Calculation) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Load Calculation Uses in Application System Selection Trees

Module Instance Name

Applications

Building Load Calculation v2

Central Heating Applications

Central Cooling Applications

To see a module's connections and how modules interact with it, view the Connections table.