The following table describes the attributes used by the Count On Inputs modules:
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Input # |
Indicates if the device status is off or on. Input # is a Binary input. |
Off |
|
Limit Variable |
Acts as a high limit in the number of devices that are able to run. Limit Variable is a floating value. |
8 |
|
Output (Float) |
V |
Indicates the current number of devices that are ON. |
0 |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)