Module Use in Applications (Preheat Pump Low OA Alarm) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use individual modules in this group using the names in the following table.

Table 1. Preheat Pump Low OA Alarm Uses in Application System Selection Trees

Module Instance Name

Applications

Preheat Pump Low OA Alarm

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

AHU 100% Outdoor Air Single Duct Applications

AHU 100% Outdoor Air Dual Duct Applications

AHU Multizone (Mixed Air Dual Duct) Applications

To see a module's connections and how modules interact with it, view the Connections table.