The following table describes the attributes used by the Latching Alarm Manager modules:
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Cascaded OR Input |
Provides the functionality to connect multiple modules using the OR operator on more than four inputs. |
Normal Set Name: Normal/Alarm |
|
Input X |
Indicates the inputs to this module (X is 1-4). |
Normal Set Name: Normal/Alarm |
|
Maintenance Switch |
Provides the result of the latch and OR operation, but is translated into the disabling/enabling of the maintenance switch. |
Enable Set Name: Disable/Enable |
|
Output |
G, V |
Provides the result of the latch and OR operation. |
Normal Set Name: Normal/Alarm |
Rest X |
Provides the inputs (X is 1-4) to return the Output to Normal when the Setup X attribute is set to Manual. |
Off Set Name: Off/Reset |
|
Setup X |
Indicates the latch action used by the specific input (X is 1-4). When the Setup X attribute is set to Automatic, the Output is Alarm if the associated input is Alarm, and equals Normal when all input values are Normal. When the Setup X attribute is set to Manual, the Output is Alarm if the associated input is Alarm, and equals Normal when all input values are Normal and the Reset n input is set to Reset. |
Automatic Set Name: Reset Type |