Viewing and Modifying Break Condition Details - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. To modify a break condition, select the break condition text (similar to a hyperlink) in the Break Condition dialog box.
  2. To enable the break condition, select the Enable check box. To disable the break condition, clear the Enable check box.
  3. To change the break condition object or attribute, do the following:
    1. Click the ellipsis (...) to browse and select the break condition Variable. The Select Reference screen appears.
    2. In the Filter box, type part or all of the object name to filter the results.
    3. Select the object that you want.
    4. Click OK.
    5. Enter the Criteria and Value for your Variable object and click Update Break Condition.
    Notes:
    • The default setting shows only BACnet exposed points. To show all points, click Show All.
    • Break conditions can also be viewed and modified by clicking the View Break Conditions button from the Simulation Control Bar while in Simulation mode.