Simulation Screen - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See the Starting Simulation section.

Table 1. Simulation Parameters

Field

Description

Startup Value

Startup values for the inputs of the application.

Item

Name of the item.

Value

Item’s starting value.

Units

Item’s starting units.

Speed x Realtime

Use to indicate the speed of the simulation. The speed range is 1–10 times real time.

Starting Simulation Engine Status Bar

Indicates the progress of entering Simulation mode.

OK

Starts simulation and closes the dialog box.

Cancel

Closes the screen without applying the changes.

Opens the Help system.