Command Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See the Commanding Items and Commanding Network Inputs and Network Outputs sections.

Table 1. Command Dialog Box

Field

Description

Attribute Command

Use to enter a value to send a test or restore the value.

Attribute Use to choose the attribute to command from the drop-down list box.
Details Shows the value entered for the test command.
Test Use to test a value for the command.
Value Use to enter the value for the test.
Restore Restores the value to the default.

OK

Opens a second screen with more command choices based on your selections.

Cancel

Closes the screen without applying the changes.

Opens the Help system.