Break Condition Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See the Simulation Break Conditions section.

Table 1. Simulation Debugging Dialog Box
Field Description

Opens the Help system.

Add

Use to add a break condition and opens the Break Conditions dialog box.

Break Conditions Table
Rule Displays existing break conditions.
Active The Active icon () is only visible when the break condition has been reached through system simulation.
Enabled Displays break conditions that are applied to the current simulation testing.

Clicking the Trash icon deletes the break condition.