Exporting Localization Preferences - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Procedure

  1. On the desired tab of the Preferences - Localization screen, click Export. The Save dialog box appears.
  2. Keep the default file name or adjust the name to indicate a specific site or use.
    Notes:
    • The default file name for each tab is listed in the Import and Export Preferences section.
    • It is not necessary to export/save a separate copy of the Johnson Controls standard preferences because the Reset and Reset All functions reset the preferences to the Johnson Controls standard default values regardless of user session.
  3. Keep the default location to save the file or adjust it as desired.
    Note: The default location is C:\ProgramData\Johnson Controls\MetasysIII\<Product Name>\UI\i18n_user_modified\com\jci\resources
  4. Click Save. The file saves and you can access it from the same computer for later use or you can copy the file to use on another computer.