Preferences - System Selection Screen - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See Setting Default System Selection Preferences.

Table 1. Preferences - System Selection Screen

Field

Description

System Selection Tree Navigation Panel

System Selection trees available. For information on the system types, see the Applications section. For information on the System Selection Wizard, see System Selection Wizard in the Configuring a System section.

Display Panel

Selected tree and allows you to make changes to the default selections. See the Setting Default System Selection Preferences section.

Reset

Resets the selected tree to the Johnson Controls standard default tree values. See the Resetting System Selection Preferences section.

Import

Opens a saved System Selection tree preference file and poplulates the screen with its data. See the Import and Export Preferences section.

Export

Saves System Selection tree preferences to a file so you can access it from the same computer for later use or you can copy the file to use on another computer. See the Import and Export Preferences section.

Save

Applies the changes and closes the Preferences - System Selection screen.

Close

Closes the Preferences - System Selection screen without applying the changes.

Opens the Help system.