Sideloop Signal Conditioning - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
These modules allow you to use multiple analog inputs with a single sideloop output controller. They provide the ability to average the inputs, add the inputs together, select the maximum value, and select the minimum value. The Flow Calculation module is described elsewhere. It allows you to convert an analog value representing velocity pressure into flow.