This module is responsible for determining the minimum flow setpoint (heating and cooling) according to the occupied and warmup/cooldown conditions. During conditions of Standby, the unoccupied flow setpoints are issued. During conditions of Unoccupied, the unoccupied flow setpoints are also issued unless there is a warmup/cooldown mode. During conditions of Occupied or Bypass, the occupied flow setpoints are issued, including adjustments made by the reset scheme.
You can view and modify the modules in this group’s logic.