Table 1 describes the attributes used by the Setpoint Reset by OA modules.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Effective Setpoint |
G, V |
Indicates the setpoint calculated by adding the Setpoint Offset to the Setpoint. |
0 °C, 0 °F |
OA High Setpoint |
Indicates that when the outdoor air temperature is this value, the Setpoint Offset is the Setpoint Span. |
21 °C, 70 °F |
|
OA Low Setpoint |
Indicates that when the outdoor air temperature is this value, the Setpoint Offset is the Setpoint. |
0 °C, 32 °F |
|
OA Temperature |
Indicates the outdoor air temperature. |
22 °C, 72 °F |
|
Setpoint |
Determines the value of the Setpoint Offset when the outdoor air temperature is at the OA Low Setpoint. |
0 °C, 0 °F |
|
Setpoint Offset |
Indicates the setpoint offset as determined by this module based on the outdoor air temperature. |
6 °C, 11 °F |
|
Setpoint Span |
Determines the amount by which to adjust the Setpoint when the outdoor air temperature is at the OA High Setpoint. |
6 °C, 11 °F |