Attributes (Pressure Request Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Pressure Request Determination module.

Table 1. Pressure Request Determination Attributes

Name

Type 1

Description

Default Value

CD Percent

 

Represents the cooling damper command.

0% open

Differential

 

Indicates the required reduction in damper command before pressure request is no longer required.

10%

Flow Request

G

Indicates the output of the module:
  • 1: additional flow is required
  • 0: additional flow is not required

0

HD Percent

 

Represents the heating damper command.

0% open

Setpoint

 

Indicates the maximum damper command that initiates an increase in static pressure.

95% open

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)