The application System Selection trees use individual modules in this group using the names in Table 1.
Module Instance Name |
Applications |
---|---|
Cold Deck Discharge Air Setpoint Reset |
AHU Mixed Air Dual Duct Applications |
Discharge Air Setpoint Reset |
AHU Mixed Air Single Duct Applications |
Hot Deck Discharge Air Setpoint Reset |
|
Hot Deck Discharge Air Setpoint Reset by EA-T |
|
Hot Deck Discharge Air Setpoint Reset by RA-T |
To see a module's connections and how modules interact with it, view the Connections table.