Discharge Air Setpoint Reset - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This module is designed to reset the discharge air temperature setpoint based on a reset process variable (typically the outdoor air temperature). The module has two inputs that define the temperature reset band (OA Reset A and OA Reset B), and two inputs that specify the DA-T setpoints at each end of that band (Discharge Air Low Limit and Discharge Air High Limit). This module has an output for the DAT-SP (Discharge Air Temperature Setpoint).

You can view and modify the modules in this group’s logic.