Attributes (Discharge Air Setpoint Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1 describes the attributes used by the Discharge Air Setpoint Determination modules.

Table 1. Discharge Air Setpoint Determination Attributes

Name

Type 1

Description

Default Value

DATCLGUNOCC-SP (Unocc Cooling Setpoint)

 

Contains the Discharge Air setpoint used when unoccupied cooling or Cooldown is required.

13 °C, 55 °F

DATHTGUNOCC-SP (Unocc Heating Setpoint)

 

Specifies the Discharge Air setpoint used when unoccupied heating or Warmup is required.

32 °C, 90 °F

EFFDAT-SP (Discharge Air Setpoint)

G, V

Indicates the effective Discharge Air Temperature Setpoint.

13 °C, 55 °F

Occ Setpoint

 

Contains the Discharge Air setpoint used when unoccupied control and WarmupCooldown are not required.

13 °C, 55 °F

Unocc Status

 

Current unocc status. This input indicates if unoccupied cooling, unoccupied heating, or neither is required.

Unocc Ctrl Not Req’d

Set Name: Unocc Status

WarmupCooldown

 

Indicates the current warm up or cool down status of the application.

Normal

Set Name: OST Warmup Cooldown

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)