Module Use in Applications (Degrees to Direction) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Degrees to Direction Uses in Application System Selection Trees

Module Instance Name

Applications

Wind Direction Determination

Custom and Monitoring Supervisory Control Only Applications (Custom Applications)

To see a module's connections and how modules interact with it, view the Connections table.