Attributes (Degrees to Direction) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Degrees to Direction modules.

Table 1. Degrees to Direction Attributes

Name

Type 1

Description

Default Value

Input

 

Indicates the angular wind direction to convert to compass points.

0

Display Units: deg angular

Wind Direction Long

G

Provides the spelled out compass point values:

  • 0=North
  • 1=NorthNorthEast
  • 2=NorthEast
  • 3=EastNorthEast
  • 4=East
  • 5=EastSouthEast
  • 6=SouthEast
  • 7=SouthSouthEast
  • 8=South
  • 9=SouthSouthWest
  • 10=SouthWest
  • 11=WestSouthWest
  • 12=West
  • 13=WestNorthWest
  • 14=NorthWest
  • 15=NorthNorthWest

North

Set Name: Wind Direction 16

Wind Direction Short

 

Provides the abbreviated compass point values:

  • 0=N
  • 1=NNE
  • 2=NE
  • 3=ENE
  • 4=E
  • 5=ESE
  • 6=SE
  • 7=SSE
  • 8=S
  • 9=SSW
  • 10=SW
  • 11=WSW
  • 12=W
  • 13=WNW
  • 14=NW
  • 15=NNW

N

Set Name: Wind Dir 16

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)