Reliability (WarmupCooldown Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1. WarmupCooldown Determination Reliability

Input

Behavior When Input Is Not Reliable

Supply Air Temperature

Automatic Warmup activation is disabled and the module only passes through the network warmupcooldown mode input.

Zone Temperature

Automatic Warmup activation is disabled and the module only passes through the network warmupcooldown mode input.