Module Use in Applications (Staged Device Enable Determination Series) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use individual modules in this group using the names in Table 1.

Table 1. Staged Device Enable Determination Series Uses in Application System

Module Instance Name

Applications

Staged Device Enable Determination Series

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.