Staged Device Enable Determination Parallel - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This module generates a True, False, or Fault state to indicate to a parallel staged device that the airflow requirements have been met. For a parallel device (a parallel fan in a single duct VAV box application), the only requirement to enable the device is that the fan is commanded on.

You can view and modify the modules in this group’s logic.