Module Use in Applications (Flow Status Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group with the names in Table 1.

Table 1. Flow Status Determination Uses in Application System Selection Trees

Module Instance Name

Applications

Airflow Status Determination

Fan Coil Applications

Heat Pump Applications

Unit Ventilator Applications

To see a module's connections and how modules interact with it, view the Connections table.