Module Use in Applications (Dual Fan Status Alarm Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Dual Fan Status Alarm Determination Uses in Application System Selection Tree

Module Instance Name

Applications

Dual Supply Fan Status Alarm Determination

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

Dual Relief Fan Status Alarm Determination

AHU Mixed Air Single Duct Applications

Dual Return Fan Status Alarm Determination

AHU Mixed Air Single Duct Applications

Dual Exhaust Fan Status Alarm Determination

AHU 100% Outdoor Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.