Module Use in Applications (Economizer Availability) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in Table 1.

Table 1. Economizer Availability Uses In Application System Selection Trees

Module Instance Name

Applications

Economizer Availability Determination

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

AHU Multizone (Mixed Air Dual Duct) Applications

AHU Rooftop Unit Applications

Heat Pump Applications

Unit Ventilator Applications

To see a module's connections and how modules interact with it, view the Connections table.