Module Use in Applications (Damper Trouble Detection) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual Damper Trouble Detection modules in this group using the names in Table 1.

Table 1. Damper Trouble Detection Uses in Application System Selection Trees

Module Instance Name

Applications

Cold Deck Damper Trouble Detection

VAV Dual Duct Applications

VAV Slave Dual Duct Applications

Exhaust Damper Trouble Detection

VAV Single Duct Applications

VAV Dual Duct Applications

VAV Slave Single Duct Applications

VAV Slave Dual Duct Applications

Hot Deck Damper Trouble Detection

VAV Dual Duct Applications

VAV Slave Dual Duct Applications

Supply Damper Trouble Detection

VAV Single Duct Applications

VAV Slave Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.