The following table describes the attributes used by the PCHWP dP Setpoint Reset By Coil Position modules:
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
CHW Coil nn Position |
Indicates the valve positions of the chilled water (CHW) coils. |
95% |
|
Effective dP Setpoint |
G |
Provides the building's CHW differential pressure setpoint as determined by this module based on the valve position of the coils. |
34.0 kPa, 5.0 psi |
Enable |
Provides the enable input, which allows the process to run. |
False |
|
Maximum dP Setpoint |
Resets the Effective dP setpoint up to the Maximum dP Setpoint. |
276.0 kPa, 40.0 psi |
|
Minimum dP Setpoint |
Resets the Effective dP setpoint down to the Minimum dP Setpoint. Set this attribute to a value such that when the value is reached and the bypass valve is fully open, the system still meets the largest minimum flow requirement required by the chillers. |
34.0 kPa, 5.0 psi |
|
Period |
Indicates the time, in minutes, that the calculation executes. |
5 minutes |
|
Stage Down Threshold |
Indicates the amount that is subtracted from the current CHW Pressure setpoint when the maximum valve position is less than 90% or is determined to be an outlier. To avoid changing the valve positions too much or too little during a stage down event, set the Stage Down Threshold to approximately 10% of the expected operating point of the building differential pressure. The default value of 2.0 psi works well for building dPs around 20.0 psi. |
14.0 kPa, 2.0 psi |
|
Stage Up Threshold |
Indicates the amount that is added to the current CHW Pressure setpoint when a valve is fully open and not determined to be an outlier. To avoid changing the valve positions too much or too little during a stage up event, set the Stage Up Threshold to approximately 10% of the expected operating point of the building differential pressure. The default value of 3.0 psi works well for building dPs around 20.0 psi. |
21.0 kPa, 3.0 psi |
|
Startup Value |
Indicates the initial plant CHW differential pressure setpoint. |
103.0 kPa, 15.0 psi |