Attributes (Flow Direction Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by this module:

Table 1. Flow Direction Determination Attributes

Name

Type 1

Description

Default Value

Flow Direction

 

This input is the direction of the flow. It is used when a directional flow BI is included in the system.

Normal

Set Name: Polarity

Flow Input

 

This input is the measured flow through the decoupled flow loop. This input may or may not have direction associated with it.

0.0 gpm, 0.0 L/s

Display Precision: 1s

Present Value

 

This output is the decoupled flow merged with flow direction. A negative flow represents flow in the reverse direction.

0.0 gpm, 0.0 L/s

Display Precision: 1s

1 B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)