Device Alarm - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Device Alarm module provides the ability to latch Input 1 through Input n. If any of the latched results of Input 1 through Input n are in an alarm condition, then the Output is Alarm and the Maintenance Switch is set to Disable. When the latched results of Input 1 through Input n are Normal, then the Output is Normal.

When Setup n is set to Automatic, the latched result of Input n is set to Alarm when the input is at Alarm. The latched result is set to Normal when the input is Normal.

When Setup n is Manual, the latched result is set to Alarm when the input is at Alarm. The latched result is set to Normal when the input is Normal and the Reset n input is Reset. Figure 1 graphically conveys the behavior of the Device Alarm module for an instance defined for four devices.

Figure 1. Device Alarm

You can view and modify the modules in this group’s logic.