Chiller Percent Load Setpoint Reset - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Chiller Percent Load Setpoint Reset module provides the Upper and Lower Percent Load Setpoints for the Chiller Selector. This module provides two float outputs, one for the Upper Percent and another for the Lower Percent setpoint. Based on the inputs, the module spans the Outputs between a high and low range. This module is implemented as a Hybrid activity.

Figure 1. Chiller Percent Load Setpoint Reset