Position Adjust Output Object - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Position Adjust Output (PAO) object drives a floating/3-wire actuator that does not provide position feedback. The object estimates the position of an actuator and then uses overdrives to reduce the difference between actual and desired (Present Value (Appears as I1)) actuator position.

You can use the value of this object in logic and to monitor the status of hardware.

For more information on the Position Adjust Output object, see Position Adjust Output Attributes and Position Adjust Output Commands.