Configuring Associated Perspectives Per Application - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Procedure

  1. In the Perspective Management window, click the System Configurations tab.
  2. In the left pane, select any configuration, such as Fan Coil, or folder of configurations, such as VAV.
  3. In the right pane, select or clear the check boxes for the perspectives that you want available for that application. You can also right-click a perspective or a column heading and click Select All or Deselect All.
    Note: Perspectives are listed in alphabetical order. To reverse the order, click the Perspective column heading.
  4. Once you have completed your selections, click Close.